Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Crane system

Pre-harnessed cable carrier system in heavy duty use for 12 years

readychain® pre-harnessed cable carriers

Any moving production at this concrete processing plant uses pre-harnessed cable carriers. In this tough environment, igus® cable carriers perform a crucial task in keeping the plant’s indoor crane and portal robot functioning.

Purchasing a completely pre-assembled system shortened installation time and prevented unnecessarily long production downtimes. The cable carriers have had no problems over a 12-year period.
readychain® pre-harnessed cable carrier Stable even under the harshest application conditions: the cable carriers are almost indestructible and are extremely resistant to wear.

Downtime reduced to a minimum

The cable carrier system reduced downtimes to a minimum for the two gantry cranes equipped with gripper robots and also set new standards for power supply within the factory. The entire production line is fully automated and conducted to the farthest end of the facility with these two cranes, which run on rails mounted alongside the hall.

Trailing cables supplied power until 1993. However, this led to repeated operational interruptions. At more or less regular intervals, the entire plant had to be shutdown. The costs involved with doing this were in addition to the cost-intensive maintenance involved with replacing cables.
readychain® Casting molds for house and garage walls are transported from workstation to workstation with special lift trucks run on rails. The power supply is conducted through energy chains

More on the products used

More cable carrier application examples from different industries



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302