Martin Raak, robolink product manager, reports on current product developments here.
Martin Raak, robolink product manager, reports on current product developments here.
After having successfully passed tests in rough vacuum on 20/10, now there is also a result for the applicability in fine vacuum.
Certificate and test result as PDF document.
After the single joint won an award in 2010, the compact robolink drive unit also received the renowned iF Design Award.
Politecnico di Torino uses a robolink 4-axis arm with drive unit and angle sensors and executes movements with "voice control".
At the Motek'11 in Stuttgart, a rotary joint was presented, which extends the operating range of the existing double-jointed arm. The new rotary joint can turn +/-90° and is intended as first axis in an articulated arm.
The arm is equipped with a single-piece pneumatic gripper made of PA2200 as a prototype. The entire moving 6-axis arm weighs significantly less than 1 kilo, and can handle about 0.5 kg.
Recommended price of 5-axis arm (without grippers, sensors) = € 1,700
Price for a complete drive unit based on step motor (NEMA23) with 5-axis articulated arm: € 5,934
Technical University of Munich, Department of Aerospace Engineering - LRT - tests the joint in rough vacuum and certifies full functionality.
Experimental conditions according to the attached certificate, test set-up documented in the film.
The high speeds of the robolink joint are tested with this testing system. The four degrees of freedom of the double joint are accelerated to an angular velocity of 150°/s. The average speed of the mounted weight (560 g) is thereby 1.05 m/s.
The application of robolink in machine tools and the influence of coolants/lubricants is demonstrated here.
This cyclic fatigue test has already run more than 2.9 million cycles and shows no damage whatsoever.
Asymmetric pivot angle arrangement: Displacement of the pivot angle of +/-90° to +130°/-50°
This gives you a completely new area of operations with our robolink multi-axis joints.
All other properties do not change compared to the original version. Both versions can be freely combined as desired.
The AS5304A linear encoder chip of the manufacturer Austriamicrosystems is located on the sensor boards.
The magnetic rings have 31 pole pairs (pivot) and 29 pole pairs (rotation), so that 4960 (pivot) and 4640 (rotation) signals respectively are issued per rotation. This corresponds to an angular accuracy of approx 0.07°. In addition, our magnetic rings are provided with an extended south pole for the absolute zero position (hall sensor). The two sensor boards are wired as follows:
| black | GND |
| red | + 5V |
| blue | Encoder Channel A |
| yellow | Encoder Channel B |
| green | Encoder Index |
| white | Hall Sensor (zero position) |
| pivoting motion | |
| red | + 5V |
| black | GND |
| white | Hall sensor |
| green | Encoder Index |
| blue | Encoder Channel A |
| yellow | Encoder Channel B |
| rotation | |
| white/brown | + 5V |
| Brown | GND |
| Gray | Hall sensor |
| white/green | Encoder Index |
| violet | Encoder Channel A |
| pink | Encoder Channel B |
Readout unit with display of the rotating and pivoting motion.
Sensorchips for
Rotating and
2pivoting motion
Magnetic rings for
Rotating and
2pivoting motion
A Bowden cable is a moving machine element to transmit a mechanical movement or a pulling force through a combination of a wire and a casing sturdy in the running direction ("draw wire" according to DIN 71986).
The Bowden cable was named after its inventor Ernest Monnington Bowden (1860-1904).
An optimized friction pair between the drive wire and the outer slide segments is achieved by appropriate materials. A support or guiding element is not necessary, because the system is self-centered in the draw wires by tensile forces. All materials, outer slide segments and wires are made of plastic. The individual outer slide segments are made of PA2200 plastic. All the individual parts are similar, they are assembled in the pre-assembly by simple clipping. The components of the outer slide have a spherical bearing face for:
Centering of the segments among each other
Transfer of pressure forces in the Bowden
3-dimensional movement potential of the segments
With the new product configurator, you can now request for a customized system quickly and easily.
Configure individually from the robot joint kit and inquire or order directly online.
robolink news and line extentions, more joints, connecting pipes and much more…
Robolink has been awarded by the "iF Forum Design GmbH" in the category "industrial design". The iF awards are given particularly to innovative and visually appealing products. As one of the oldest competitions, the iF award is an internationally recognized design award.
angular sensor Due to the integrated angular sensors, an arm can also be used directly as "teach-in" arm. Read-out angle information can be saved and called up or even directly transformed into movements (see film). Currently the sensor technology is advanced for series production.
Evologics plant: the torso. Each arm has 7 degrees of freedom, 4 of them in the respective 2 robolink joints. Each arm is driven by 7 DC motors; they are stationary in the "breast area".
Due to the decoupling of the drives from the moving arms, each arm only weighs a little over 1 kg. Load capacity per arm is also 1 kg with very high dynamics (see film). Result: a load to dead weight ratio of 1:1 becomes possible!
The robolink highlights at the Hannover Messe 2010 - round tour through the stand and presentation of novelties.
Increase in the transmitted torque (rotation) from 5 (generation 1) to 7 Nm (generation 2) in continuous operation. (Damage in the one-off fracture test at > 24 Nm)
GFRP and CFRP rods now available in profiled version. Maximum length of 1 m. See price list. Weight CFK: 170 g/m, GFK: 200 g/m, Aluminum 270 g/m
Our beta tester special offer has been running since the end of December. So far approx. 30 customers have been sent samples and approx. 20 customer-specific tests are running.
Read more
The revised, new version of the articulated robot joint is now available as a prototype. The following product improvements have been achieved:
Read more
The articulated joint has the basic dimensions shown below:
We originally wanted to manufacture injection molded tools in connection with the HMI in order to produce the product as shown.
Read more
Multiple-axis joint for robots - Find out more about the use of the first robolink prototypes.
Your contact
Martin Raak +49 (0) 22 03-96 49 409 Your requirements?
myigus myCatalogHomeProduct configuratorOnline catalogFrequently Asked QuestionsApplication examplesStatus of product developmentTestlabDownloadsEmail the product expert
More than 80,000 products available! Delivery and consultation Mon-Fri from 8am-8pm and Sat from 8am-12pm!
Terms and Conditions Imprint General Information