Video of the Week – How to save time and space with igus® readychain® module connect13/12/2018

Module connect is a new kind of plug-in connector from igus for connecting different electric cables, fibre optic cables and pneumatic hoses. It’s simple, modular design, creates a unique connect/disconnect point with a single module consisting of several different connector inserts. Used as part of a readychain, it connects several cables in the smallest of installation spaces, in one go. As you can see in this week’s video, the housings can then be joined together to create an almost unlimited number of module variations. The low profile saves space, achieves a high contact density. Another advantage is that the integrated honeycomb strain relief system from igus works alongside to ensure secure cable fixation. Module connect can be adapted to fit any e-chain no matter what the application, whether it’s at the fixed end or moving end of an e-chain, between two e-chains or for routing cables into terminal boxes or switch cabinets. To watch the video about readychain module connect, please follow this link: www.igus.co.uk/readychainmoduleconnect. For more information about readychain, please visit: ww.igus.co.uk/readychain or call igus directly on 01604 677240.