Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
![]() |
New chainflex® hybrid cables for SEW and Siemens motors available with 36-month guarantee11/06/2019
igus has developed the CF280.UL.H, a new hybrid cable for SEW and Siemens motors, designed for use for use in energy chains. Engineers working in intralogistics, machine tool construction or the automotive industry have the added benefit of purchasing the chainflex cable with a 36-month guarantee, either bought by the metre or supplied as a ready-to-connect readycable. The CF280.UL.H hybrid cable is suitable for applications down to a bend radius of 10x diameter in temperatures ranging from -25ºC up to +80ºC. Depending on the manufacturer's specification, the cable has a black or orange oil-resistant PUR outer jacket, is coolant-resistant and flame-retardant. A braided shield with high coverage ensures good EMC protection over a long service life. igus regularly carries out continuous in-house tests on all its cable ranges. In a series of tests at 7.5x diameter, the CF280.UL.H hybrid cable lasted over 8 million cycles without damage. Another advantage of the new cable series is that it has UL approval for use in North America, as well as EAC and CTP certification for the Russian market. Due to customer demand, igus offers all its cables as readycable with the appropriate connectors pre-assembled. With more than 4,200 drive cables available made in line with to 24 manufacturers’ standards, engineers will always find the most cost-effective cable for their application. All cables are tested after harnessing and receive an igus seal of approval. By testing all chainflex cables under real conditions, igus is in the unique position to offer a 36-month guarantee. For more information about the full range of chainflex cables from igus, please visit: www.igus.co.uk/chainflex or call igus directly on: 01604 677240 |