New generation E4Q energy chain from igus® for unsupported and long travels25/06/2019

Inspired by nature, designed for industry: this is the new E4Q energy chain from igus for unsupported and long travels. The chain links of the e-chain have a pebble-shaped design for weight reduction and a completely new crossbar locking concept, which enables the energy chain to be assembled by hand in seconds. On the upper side of the crossbar there are two recesses through which the locking hooks can be pulled open. Once unlocked on both sides, the crossbar can be lifted off. This makes it easy to open and close the chain, even when fitted inside a guide trough, and speeds up assembly by up to 40%. The new crossbar has significantly higher pull-out forces in the locked state compared to similar e-chains in the range. A further advantage of the E4Q energy chain is that with the optional noise dampeners fitted, it offers very quiet operation. This is achieved by attaching rubber elements to the horizontal stop-dogs, additionally dampening the impact noise of the already very quiet e-chains. These can be retrofitted at any time. For more information about the E4Q energy chain, please visit: http:// www.igus.co.uk/E4Q or call igus directly on:01604 677240