igus® drylin® delta robot is now on tour up and down the country24/07/2019

With live performances at business venues up and dow¬¬¬¬n the UK and Ireland the igus drylin delta robot is now officially on tour. You may have missed its recent dates in Aberdeen and Bristol and, in Ireland, Dublin and Galway but fear not – further dates the next three months are scheduled in the East Midlands, Gloucestershire, Wales and the South East. The drylin delta robot uses NEMA stepper motors and encoders to ensure fast handling of up to 1 kg with a precision of ±0.5 mm and for loads up to 5 kg there is a guaranteed pick rate of at least 60 per minute. The open design enables manufacturers to use their own controller, however, they can opt for the intuitive and easy-to-use dryve D1 controller from igus. About the success of the tour Vanessa Whiteley, drylin delta business development manager at igus, says: “Proud to be known for our tactile and practical approach to engaging with our audience, we’ve already added more dates this year.” There are some secret dates too, to find out more, please contact Vanessa Whiteley at: vanessa.whiteley@igus.net or call igus directly on: 01604 677240