Shock-resistant polymer bearings for tine arms in rotary swather

Tribologically optimised polymer plain bearings have proven themselves in harsh outdoor use for many years.

What do protesting dairy farmers and the agricultural machinery industry have in common? They are under high cost pressure. As a result, investments in agricultural technology must bring significant improvements for relatively little money. In the following example, tribologically optimised polymer plain bearings - special bearings - provide a form-fit connection on a standard component, the core of the machine. For many years the plastic plain bearings have been proving their worth in arduous field work.

Profile

  • What was needed: iglidur G plain bearings
  • Requirements: Continuous load of the plain bearings during peak season; high availability; high radial forces require shock-resistant and tough bearings; adverse environmental conditions such as dust and dirt; long service life with possible corrosion of the steel parts
  • Industry: agriculture
  • Success for the customer: The system has been working smoothly since the start of volume production; wear has been significantly reduced compared to plain bearings made of metal; there is less noise development during operation; the economic efficiency could also be increased
FELLA harvester Four rotary rakes ensure a high area output. To ensure that they function reliably, the plastic plain bearings play an important role in the support of the prongs.

Problem

The company AGCO Feucht GmbH (at that time still Fella-Werke GmbH) has already been designing implements for tractors for more than 90 years. These include mowers, hay rakes and swathers. The swather works by using eight, ten or twelve tine arms to rake together stalk material that has already been mown or spread out to form a swathe. All swathers made by this supplier work exclusively using rotary technology, i.e. exploit the benefit of high area performance. Supporting the prongs is one of the tasks of the complex control system and is the machine's most important function. Two plain bearings are fitted to each prong. If damage occurs here, the rotary swather stops, which must not happen under any circumstances during harvest time.
During the high season in summer, agricultural harvesting machines have to work smoothly for many hours a day for a few weeks. The external stresses are extremely high. The transport of the stalk material over the ground, as well as the contact of the prongs with the ground or the approach to obstacles such as bushes, hedges and stones, primarily generates radial forces. To avoid damage to the plain bearings in these situations, they must be shock-resistant and very tough. Then there is the dust and dirt, and finally the high-pressure cleaning. Harsh operation conditions and long service life with possible corrosion of the steel parts place very high demands on the plastic plain bearings.
Lastly, the machine builder aimed to find a compact and affordable solution.

Solution

Tribo-optimised polymer plain bearings made of the special material iglidur G have been used as plain bearings for ten years now. These are economical all-round bearings which - free of lubricants and maintenance - among other things prove their strengths in simple pivoting and rotating movements, with very high loads as well as with high dirt requirements.
Since the introduction of volume production, the system has been working smoothly. The anti-rotation feature ensures a completely firm fit of the bushing in its housing. The benefits pay off for the manufacturer of agricultural machines: the amount of wear has been significantly reduced in comparison to plain bearings made of metal and less noise is generated when the equipment is in operation. Furthermore, the economic efficiency is good, since, among other things, the finishing of the housing hole for the plain bearings in the aluminium bearing tube is completely unnecessary. Thus, the plastic bearing with the conical outer side was simply adapted to the conical design of the housing hole. This also applies to the conical mounting holes of the aluminium bearing tubes, which are screwed to the tapers of the gyroscopic bells.
It quickly became clear to the company that costs could be saved with plastic. In the beginning, we turned the plastic bushings ourselves and later injection-moulded. Since the choice of material was not right, the result was not right either. The extensive igus® product range, which includes standard and customised parts, quickly provided a suitable solution. Having been tested thousands of times under everyday conditions in the igus® laboratory, the high level of abrasion resistance and the dry-operation properties of the polymer plain bearings immediately revealed their worth in real-life agricultural applications.

"We buy all components from the respective specialist, which also includes the special bearings made of plastic from igus. The share of iglidur polymer bearings will continue to increase in all machines of our product range. Their stability and cost benefits are quite simply great."
 
Dipl. Ing. (FH) Bernhard Kohl, Head of Design at FELLA-Werke GmbH
iglidur G plain bearings "iglidur G" polymer plain bearings - special bearings - are installed on the prongs of the rotary swather.
Rotary swather Each rotary swather has eight, ten or twelve prongs. The maintenance-free polymer plain bearings ensure smooth operation over a long service life of the machine.
Prong Prong with two polymer plain bearings.
iglidur G plain bearings In this "iglidur G" plastic plain bearing, a special part for FELLA, the control shafts move clearance-free.

Consulting

I would be happy to answer your questions

Shipping and consultation

In person:

Monday to Friday from 8am - 8pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH