Stick-slip-free movement: linear guide in winding machine for carbon fibre spools

With these carbon fibre spools, a drylin linear guide implements a uniform movement.

This machine is used to wind carbon fibre spools for use in aerospace technology, for example. The spools must be of high quality. Due to the very slow manufacturing process of carbon fibres, the speed of this movement is extremely low. A drylin T linear guide was selected, with which a sufficiently uniform linear movement can be achieved for this application at the low speeds.

Profile

  • What was needed: drylin T linear guide system
  • Requirements: Due to the very slow manufacturing process of carbon fibres, the speed of this movement is extremely low. A low breakaway torque (stick-slip) and minimal clearance were crucial for the linear guide.
  • Industry: Aerospace, aviation
  • Success for the customer: Preliminary tests at the customer's site proved that the drylin T achieves a sufficiently uniform linear movement even at extremely low speeds. The guide carriages consist of lubrication-free and extremely durable sliding elements.
Carbon fibre pool

Problem

Carbon fibres are becoming increasingly important in technical applications, e.g. in aviation and aerospace technology. For further processing into fabrics or braided sleeves, it is necessary to wind up the fibres after the manufacturing process. The quality of these spools is crucial for further processing. The company Georg Sahm GmbH & Co KG from Eschwege has therefore decided to develop a winding machine with automatic change function, with which carbon fibre spools of a high quality can be produced.
A uniformly controllable contact pressure of the filament guiding device on the winding material is an important parameter for achieving a high spool quality. The filament guide moves linearly upwards with increasing spool diameter. Due to the very slow manufacturing process of carbon fibres, the speed of this movement is extremely low. A low breakaway torque (stick-slip) and minimal clearance were important criteria for the design of the linear guide.

Solution

Preliminary tests at Sahm proved that the drylin T linear guide system can achieve a sufficiently uniform linear movement for this application, even at extremely low speeds. It thus prevents the stick-slip effect so that the filament guide can move continuously upwards in a linear fashion. Due to the adjustment possibility of the guide carriages, an almost clearance-free fine adjustment of the guide is possible. A defined displacement resistance of the guide has been set for this adjustment.
The core of the guide carriages consists of lubrication-free and extremely durable sliding elements made of our high-performance polymers. They are quick and easy to handle and maintenance-free in use. The rail guides made of hard anodised aluminium are tough and corrosion-resistant.

Carbon fibre pool
Carbon fibre pool

Markus Ludwig, Georg Sahm GmbH & Co KG, Eschwege

Further interesting applications from extremely diverse areas can be found here.


Go to manus® contest


Consulting

I would be happy to answer your questions

Shipping and consultation

In person:

Monday to Friday from 8am - 8pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH