The igus® e-spool® cable retractor reel safely guides many different cables in a confined space.The e-spool® cable reel uniquely combines two different energy supply systems: one standard energy chain is guided by a roller, providing the correct length and tension of the energy supply system through an integrated spring. In the home position, the energy chain is completely rolled up to save space. The twisterband connects the roller with the shaft end block, serving as an interface to the supply side cables.
Cable reeling drums are typically found in the grid section of the theatre / Auditorium, Floor mounted then using a bespoke roller system and guide hole through the grid floor, the cable management system is then connected to the ladder truss / Bridge.
Our e-spool® uses our twisterband which is fixed on the side of the cable drum, acting as a secondary cable management system. The twisterband offers great rotation movement in very small spaces so, the e-spool® can be used in a confined area as well as offering a hardwired maintenance free cable management system.
Monday to Friday from 8am - 8pm.
24h