e-cord micro modular guide system for cables <3mm

Three-dimensional movement with low installation height requirements

Safe and flexible guidance of the smallest hoses Ø <1mm is the functional description of the innovative igus energy supply system e-cord micro. The flexible e-cord micro has a modular design and can thus be customised to the movement in the machine. The predefined radii prevent the hoses from kinking and ensure a smooth process without machine downtime.
 
  • Safe guidance of the smallest hoses
  • Has a modular design and can thus be customised to the movement in the machine
  • Predefined radii prevent the hoses from kinking

The actual capillary tube is only as big as the needle of a syringe. The capillary tube must not be bent to a radius of less than 45mm so that it can be moved dynamically in the long term. The e-cord micro was developed for this purpose. The capillary tube is first placed in a hose, which is then clipped into the holder. The flexible system now allows movements in several axes and the radius of 45mm is consistently given.
 
Request a project with e-cord micro now
e-cord micro 1) Connection piece
2) Curved element R
3) Adaptation to pipettes
4) Straight intermediate piece
e-cord micro A) Clip-in function 3mm
X) Min. 30mm, depending on travel
R) Curved element >=45
H) 70mm

Consulting

I would be happy to answer your questions

Shipping and consultation

In person:

Monday to Friday from 8am - 8pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH