New CAT5e and CAT6 cables for use in e-chains, with approval for the American market07/05/2019

CAT5e or CAT6 cables are vital for the implementation of Industry 4.0 in automation around the world. The new igus chainflex CFBUS.045 (CAT5e) and CFBUS.049 (CAT6) Ethernet cables, have earned an enhanced UL listed mark for use in North America at 600V. “If there are test certificates for the cables, the time and effort required for customs clearance and commissioning reduces drastically,” explains Justin Leonard, the-chain director, igus. The special braided shielding of these cables provides high EMC (electromagnetic compatibility) protection, which means that these Ethernet cables can be used safely alongside drive cables. They have been successfully tested in the igus test laboratory for more than 76 million strokes with a bend radius of 9.5x diameter and are available from stock from 1 metre length. With more than 1,300 types, igus offers the widest range of energy chain cables with international approvals, including UL listed cables. For exporting companies, this makes an easy market entry into the United States, because the UL (Underwriters Laboratories) is the most well-known and comprehensively accepted test organisation in the USA. It regularly publishes standards and certifies products, such as the igus cables. For more information about the chainflex CFBUS range of bus cables: www.igus.co.uk/igusCFBUScable or call igus directly on: 01604 677240