Mobile power socket supplies container ships at the Port of Hamburg with shore power

Three movable energy chains on the quay ensure the precise supply of energy for ships.

Profile

Application Schneider

Products used

Strain relief

chainfix strain relief

Sensors for chain/cable

Energy chains along the quay

Problem

Solution

We reduce pollutants, CO2 emissions and noise with shore power technology [wie dem iMSPO-System]. This step is particularly important in ports like Hamburg, where the harbour and the city are in close proximity to each other.

Peter Tschentscher

Mayor of Hamburg

Three mobile "sockets" (300, 150 and 110 metres long) run along the quay at Hamburg harbour and supply the docking ships with shore power.

Thanks to the flexible system, ships can moor freely along the quay and do not have to align themselves to the shore power connection.

The so-called iMSPO (igus Mobile Shore Power Outlet) consists of a mobile trolley with the socket box and energy chains that move the heavy cables safely along a rail system.

The system can be operated quickly and easily. In total, no more than two people are needed on land.

At the CTH, an iMSPO system assembled on a custom-built steel structure is used to utilise the free space above the terminal. The system was developed especially for limited space above the flood wall and where free access is required for the emergency exit on the quay.

The iMSPO received the award "Port Innovation of the Year" at the Electric & Hybrid Marine Expo Europe 2024 in Amsterdam.

Contact us

Contact details

Opening hours