The first batch of the famous all-plastic igus bicycle is in production, while igus builds a high-volume production line. The day has finally come. After months of development, the igus:bike, a bicycle made of 92% plastic with a high proportion of recycled material, is in production. The first 100 bikes are being produced while igus […]
igus launches a new lubrication-free material, for bearings needing higher running performance with high dynamic forces, ideal for heavy-duty applications. igus has developed plain bearings made from high-strength, fibre-wound materials – the igutex bearing family. These use carbon fibre embedded in the material and are used where very high impact loads occur and where injection-moulded […]
Would your company like to save multiple hours and cash for every machine you build? MACH 2024 presents Module Connect, a unique and elegant engineering design to help machine users save assembly time. Plus: not one but three low-cost robots will be demonstrated, part of the popular RBTX.com marketplace helping companies automate low-scale but precise […]