Change Language :
The bend radius is the radius at which a cable can be bent without damaging it (including kinking). The smaller the radius, the greater the required flexibility of the material. A frequently asked question in this context is: how much can we bend a cable without damaging it or impairing its function? The answer depends mainly on the particular cable being considered. There are several industry standards, such as IEEE 1185, ICEA S-75-381, ICEA S-66-524 or ICEA S-68-516, which provide minimal bend radii for many different cable types.
When choosing cables and cable carriers, consider the minimum bend radius
The minimum bend radius is the radius below which an object cannot be bent. In many installations, cable carriers are used, so the question arises: how do we select the bend radius of a cable or a cable carrier?
When deciding on a cable management system, there are several ways to extend the service life of the cable. One of the most important factors is the selection of the right bend radius for the cable carrier. It is important that the radius (except, perhaps, in space constrained applications) is greater than the recommended minimum bend radius of the cables. One of the key factors in long service life and operational reliability is choosing the right radius for the cable carrier. All cable carriers have several bend radii to choose from and each manufacturer proposes a minimum bend radius . The radius chosen for the cable carrier depends on the cable with the largest diameter.
General rules and recommendations for selecting the radius
Do not exceed the manufacturer's recommended minimum radius - but the maximum radius is optimal. Basically, cables with flexible specifications that move must be supported so that the connection points are not mechanically stressed and a sharp bend is avoided. If this is achieved by a loop, the cable must be provided with a bend radius of at least 10 times the diameter of the cable. The larger the radius, the less stress is exerted on the cables, which ensures a longer service life. It should be noted that the minimum bend radius is partially based on a temperature range for the bending. Particular care should be taken when the ambient temperature reaches or exceeds this temperature for the cable.
This is especially true for cryogenic applications where thermoplastic cables tend to stiffen when exposed to cold. Rigid cables can increase the radius of the cable carrier and lead to mechanical errors. It is recommended to use a cable with a PUR or TPE jacket at low temperature and/or to consult the manufacturer for recommendations on bend radii. For space constrained applications, the cable carrier radius must be less than the recommended minimum bend radius for the filling pack. This is not ideal, but if it cannot be avoided, cables designed specifically for low bend radius installations should be used. The igus chainflex range includes load-bearing control cables, servo and motor cables or robot cables as well as encoder cables, bus cables and data cables, which can be safely used in demanding environments and are characterised by their very long service life.
Dynamic applications with tight bend radii can quickly allow the copper cores of conventional cables to meet their mechanical stress limits. Especially in areas of application that only have a small installation space but require a high number of strokes, special igus cables offer increased operational safety.
In addition to a stranded wire in a very bend-resistant design, very abrasion-resistant and highly resistant jacket materials are used, which increase the flexibility of the cable. With its many years of experience in its own test laboratory, igus can also guarantee a long service life and planning reliability in energy chains for chainflex cables with the smallest bend radii.
The areas of application for cables with tight bend radii are diverse. They are particularly needed in applications where flexible and dynamic movements must be carried out in the smallest possible installation space. For example, they are used in the semiconductor and assembly industry, the automation industry, as well as in the automotive and banking sectors. New application possibilities arise in automatic doors for vehicles and trains as well as in automatic self-service food vending machines and the packaging industry.
Do I need a bend radius calculator? Calculating the bend radius for a cable management system can be a daunting task, but ensuring you choose correctly to maximise the service life of your cables is paramount.
We get asked a lot, “Do you have a bend radius calculator?” or “How do you measure the bend radius?” So, let’s look at answering those questions for you.
One of the most crucial factors in specifying the right energy chain system or cable carrier, as it is sometimes referred to, is ensuring you select the correct bend radius for the cables being carried. It is important to note that the bend radius of the energy chain should be larger than the minimum bend radius of the cables and media that make up the filling. There are exceptions to that rule, such as applications with space restrictions, but it must be recognised that this will reduce the service life of the services significantly.
All energy chain systems have multiple bending radii to choose from and every manufacturer should suggest a minimum bend radius. The bending radius chosen for the energy chain will depend on the largest diameter for either the cable or hose. But why do manufacturers suggest this? By selecting a larger bend radius than required, this will extend the lifespan of the cables and hoses.
Never exceed the manufacturer’s suggested minimum bend radius. Just don’t!
As mentioned previously, the larger the bend radius, the less stress is put on the cables and hoses, which will ensure longer service life.
Consider temperatures. The minimum bending radius is partly based on a temperature range for flexing; therefore, consideration is required with special environments and applications where temperatures exceed the recommendation for the cable. The same applies to extremely low temperatures. For these low-temperature applications, the cables tend to stiffen and become brittle when exposed to the cold, leading to mechanical failures.
Ensure the energy chain system is being fitted with the correct matching dynamic cables for your application.
If the application has a space restriction, the bend radius of the energy chain system may need to be smaller than that of the recommended minimum bend radius. Again, referring to previous statements, this is far from ideal but occasionally it cannot be avoided. In these special circumstances, we would recommend using cables specially designed for low-bend radius installations or consult your cable carrier manufacturer for the best solution.
Remember this is a dynamic bend radius; many cable and hose makers quote what is actually a static radius. As soon as the service is being moved dynamically, fatigue can set in and therefore the dynamic radius is typically larger (igus® cables are quoted as dynamic radius for millions of cycles).
The bend radius is defined by a point in the space at the centre and is measured to the centreline of the e-chain® (see diagram). The reason the centreline is used is that this is where the cables and hoses sit and therefore can be matched to the recommended minimums suggested by the cable manufacturer.
In most cases the minimum bend radius is expressed as a factor times the outer diameter of the service (e.g. for chainflex cables this can be from 12.5xd to as low as 4xd for our special cables).
Still not sure on the bend radius calculator? Speak to your local engineer or contact an igus® contact in the office and they will help you.