Change Language :

During the research and development phase, engineers fulfil extensive research. This is so they can gather data, highlight risks and preform tests on products to make sure they meet quality assurance standards. This will help to develop and create a well thought out strategy for building a product customers love.
At igus® we offer outstanding products tested and delivered to the highest possible standard. Take a look at our products and see what you think.
Proven, predictable, tested
Materials are manufactured by igus® in accordance with the motto “Tech up, Cost down”. Our products are designed with great passion to extend the service life of machines and applications, eliminate maintenance and reduce costs. For our engineers, the quality and safety of parts, i.e. their resilience and service life, are an important criterion in development. Every igus® product is tested thoroughly before it is made available for sale. To this end, we have been operating our own test laboratory since 1985. It not only is the largest test laboratory for tribopolymers in the industry in terms of area, but also conducts the highest number of product tests and test procedures
What is tested?
Our facilities for testing applications and materials cover a total of 3,800m². Every business sector has its own test laboratory, however we test some products together on one area. For example, 1,500m² is dedicated to testing chainflex cables in our own energy chains. For especially long travels, 2,000m² of outdoor space is available. iglidur plain bearings, drylin linear bearings, and our Low Cost Automation components are tested in an area of over 300m². The latter is tested under real conditions.
To be able to develop new cleanroom-compatible products quicker, we operate our own cleanroom laboratory with an ISO Class 1 cleanroom system in cooperation with the Fraunhofer IPA. An outdoor testing area, a laboratory for noise tests and the climatic chamber with -40°C completes our test area. To achieve maximum realistic conditions, we also test customer applications and conduct industry tests.



Research and development can vary depending on the industry however there are some fundamental key points which can explain what research and development is.
The need for development in new products, techniques, innovations and improving exisiting ones is the basis for research and development. These can be broken down into 3 categories:
You can read more about what research and development is in the engineering sector in the blog.
Why is research and development important in a business?
R&D introduces new products and services, enabling businesses to stay ahead of their competition.
Product research is important to create successful products. It helps to understand the customers needs and what they want. The research ensures them to make the correct choices to create new ideas.
Engineering focuses on solving technical problems with intelligent solutions. Therefore, research and development is crucial for technologies to keep existing systems working.

We can help you with your research and development by supplying sample boxes and sample products for you to test yourself.
Having a physical sample can be really beneficial when starting new projects and within the R&D stage, testing can be crucial.
We have a range of boxes available but if the products in the box don't quite meet your requirements, please contact us and we will do our best to send you the sample product you need.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h