Mobile shore power supply at the port of Copenhagen - saving time and increasing flexibility in daily operations

A mobile socket outlet covers the power supply at two quays over a length of up to 360 metres

Profile

Products used

Flexible shore power supply

Flexible power supply iMSPO

Energy supply on the quay

Energy chains along the quay

Problem

Solution

The socket for the cruise ships' power supply runs underground in a trough up to 360 metres long.

A 4040RHD rol e-chain transports the heavy cables several hundred metres along the quay.

After removing the base plate and raising the connection, the cables can simply be plugged in. Here is an example of an installation at the harbour in Rotterdam.

A transfer vehicle (CCM) is now connected to the mobile socket. It transfers the cable several metres upwards where it is connected to the ship.

Five igus energy chains and several chainflex cables were also installed on several transfer vehicles.

The iMSPO received the award "Port Innovation of the Year" at the Electric & Hybrid Marine Expo Europe 2024 in Amsterdam.