Mobile shore power at cruise ship terminals in the Port of Rotterdam

Movable socket provides power for ships along the 230-metre-long quay with pinpoint accuracy

Golden vector 2026

Profile

Products used

Problem

Solution

It's unique because it [ iMSPO Cruise] is a flexible system. We have a 230m trough, so they determine where the transfer vehicle goes, depending on where the hatch is located. The ship does not have to be positioned precisely. It does not matter whether the ship is moored to starboard or port.

Arjan van der Linde

Manager Cruise Port Rotterdam, Shore Power

At the cruise ship terminal in the port of Rotterdam, a movable socket for the shore power connection of the docking ships moves 230m along a trough under the quay.

The so-called iMSPO (igus Mobile Shore Power Outlet) consists of a mobile trolley with the socket box and energy chains that move the heavy cables safely along a rail system. It can be moved by two people using the remote control.

The iMSPO received the award "Port Innovation of the Year" at the Electric & Hybrid Marine Expo Europe 2024 in Amsterdam.