Stepper motor

How they work, applications and types

Stepper motor vs servo motor: choosing the right one

Servo and stepper motor comparison.
  • Precision requirements and motion type: Does your application require a high level of precision and accuracy? A stepper motor and a servo motor can be a good choice.
  • Budget constraints: If costs play a major role and moderate precision is sufficient, a stepper motor may be best suited to your requirements.
  • Complexity of control: If your team lacks experience with complex control systems, the stepper motor offers simpler implementation when using controllers such as the igus D1.

Function comparisons between servo and stepper motors

Technical specifications

Servo motor:
  • Control method: Pulse width modulation (PWM) signals, often coupled with PID controllers, control the motor position and speed
  • Feedback system: Uses encoders or resolvers for position feedback
  • Torque characteristics: Excellent torque across the entire speed range, high torque at low speeds
  • Applications: Robotics, CNC machines, automation systems with variable loads
Stepper motor:
  • Control method: Pulse signals control the motor's step sequence; microsteps can be used for smoother motion
  • Feedback system: Generally without feedback (open loop); closed-loop versions are less common
  • Torque characteristics: High holding torque at low speeds, but decreasing torque with increasing speed
  • Applications: 3D printers, laser cutters and other applications with low loads and high precision

Benefits

Servo motor:
  • High accuracy: Servo motors offer exceptional precision and repeatability, making them perfect for tasks that require precise positioning.
  • Speed and torque control: The closed system allows servo motors to maintain strong speeds and provide different torque levels, even under changing load conditions.
  • Lower heat generation: Servo motors are more efficient compared to stepper motors, resulting in less heat dissipation during operation.
Stepper motor:
  • Cost-effectiveness: Stepper motors are more cost-effective than servo motors, making them popular for budget-conscious projects.
  • Simple control system: The open loop simplifies the control system of stepper motors, which can be easily implemented without complex control algorithms.
  • Holding torque: Stepper motors can hold a position without the need for a continuous power supply, which is advantageous for static holding applications.

Restrictions

Servo motor:
  • High costs: Servo motors are generally more expensive than stepper motors, mainly due to the additional feedback devices and more complex control systems.
  • Complex control system: The configuration and adjustment of a servo motor's control system parameters can be difficult and requires expertise.
Stepper motor:
  • Limited performance at high speeds: Stepper motors can become inefficient at higher speeds due to resonance, which reduces their performance in high-speed applications.
  • Lower accuracy: Due to step losses, stepper motors may experience positioning errors under dynamic load conditions.

Browse stepper motor types

Stepper motor with shaft and connector.

Shaft stepper motor

Stepper motor with connector and visible cables.

Lead screw stepper motor

Motor with flange and shaft in front view.

Specialist stepper motor

Linear actuator with threaded spindle and motor, isolated on a transparent background.

Linear actuator

Why choose igus® stepper motors?

All electric motors are 100% tested

Delivery from 1, no minimum order quantity.

No minimum order quantity

Shipping from 24hrs and consistently maintained stock

Long product life

Frequently asked questions

Compatible products for our electric motors

dryve control software with machine configuration and connected igus drive module.

Motor controller

DLE Motorleitung with exposed multi-coloured conductors at the cable end.

Matching cables

Mean Well NDR-480-24 DIN rail power supply with terminal blocks and metal casing.

Power supplies

Additional resources

Orange keyboard key with a white contact icon and arrow, suggesting contact access.

Sample

Contact us

Whitepaper pages about selecting a drylin e motor control unit, with product photos and section headings.

Download the whitepaper

Technical resource hub

Contact us

Contact details

Opening hours