Cold-resistant and heat-resistant cables

Information on cold and hot-resistant cables

Categories of temperature resistance cables

Chainflex cables in an industrial test lab with production equipment and inspection stations.
  • igus® test in e-chains®- In this test, the cable is fitted taking into account the bend radius, the interior separation and the strain relief elements. After assembly, the cable is moved according to the igus® test standard values. The movement takes place in the climatic container at temperatures down to -40°C. The test is deemed to have been passed if the construction is removed from the e-chain intact (especially without jacket damage).
  • Flexible: test according to DIN EN 60911-504 for "moved". The cable is cooled down to test temperature. After the cable has been subjected to the test temperature for more than 16 hours, it is wrapped around a mandrel. After the removal, a pure visual inspection is carried out. This so-called winding mandrel test is considered to be passed if the jacket of the cable remains undamaged.
  • Fixed: test according to DIN EN 50305 for "fixed installation". The cable is held in place at test temperature and a test weight is dropped onto it. This so-called cold impact test is regarded passed if the cable jacket remains undamaged.

Cold-resistant and heat-resistant cables

Cable carriers on a machine frame beside a conveyor system.
bend radius

Heat-resistant cable for minimal maintenance and high functional reliability

Robotic cables and protective conduits inside an industrial machine.