Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

chainflex® creates space!


Smaller radii, smaller machines, greater freedom with drive technology

In line with current trends, modern machines are becoming ever smaller and more compact. This means smaller radii are being sought and used more and more frequently in energy chains. The challenge now is to use cables that can withstand this additional load as well as these space constraints. Customers still want their cables to last for a long time with high safety and reliability not being compromised. Standard cables cannot do this reliably.
The question is, what cables are suitable for small installation spaces and how can safety and a long service life still be achieved? 

Answer: chainflex® cables!
Visit the shop!
In this video, we explain in a clear way how we solve the space problem. See for yourself!

Cables sold by the metre

chainflex cables

Over 1,350 cables from stock, delivered in as little as 24 hours

Visit the shop

Harnessed cables

readycable

4,600 harnessed drive cables of the desired length that work with 24 manufacturer standards

Find out more

Drive cables creating space

CF38.D motor cable

  • Service life- 43 million strokes
  • 25% reduction for installation space
  • Bend radius:175mm (factor 6.5 x d)
  • XLPE core insulation
  • Advantage for the customer: higher temperature load
  • Click here for more information
Buy now

CF29.D Servo cable

  • Cable type: Halogen-free TPE
  • Service life- 45 million strokes
  • Bend radius:100mm (factor 7.2 x d)
  • Inner sheath for long travels
  • Longer durability and protection against corkscrewing
  • Click here for more information
Buy now

CF11.D encoder cable

  • Service life- 66 million strokes
  • Bend radius: 75mm (factor 7,1 xd)
  • Reduction in installation space by up to 32%
  • TPE outer jacket for extreme cold
  • Click here for more information
Buy now

CF37.D motor cable

  • For heaviest duty applications
  • Hydrolysis and microbe-resistant
  • Advantage for the customer: higher temperature load
  • XLPE core insulation
  • Click here for more information
Buy now

Reduce installation space by up to 25% -motor cables

A motor cable is a comparatively simple cable. Its only task is to supply the motor with electricity. As it is connected to a frequency converter, its voltage class is 600V/1,000V, and it has four cores (L1, L2, L3, PE). Motor cables are used where large amounts of energy are transferred; however, automation technology requirements have increased dramatically in recent years.
To meet all these requirements and stand up to the continuous mechanical load in an energy chain, materials and manufacturing processes are essential for motor cable function. Ensuring reliable drive power supply under heavy loads remains an elementary task. A harbour crane is a good example.
igus motor cables are made with special high-quality networked XLPE insulation materials. They are specifically designed for energy chains and provide low capacitance for fast, low-loss switching times and a very high insulation temperature reserve with higher current density. They must also have a long service life when used in large-scale travels or tight bends. The quality of the stranded wires in the cores must also be very high in order to move the cable continuously in small installation spaces. This ensures a long service life and reliable power supply.
Find more information about chainflex® motor cables

CF29.D servo cable drive technology

Reduce installation space by up to 32% – servo cables

Like a motor cable, a servo cable supplies the motor with power. Of course, we use the advantages of XLPE core insulation here, too. However, a servo cable also has other crucial functions: it supplies the motor brake with energy and/or carries the signal from the temperature sensor to the frequency converter. For this purpose, a servo cable has one or two additional control pairs with extra shielding so that no interference reaches the frequency converter. Servo cables often also have an overall shield to prevent electromagnetic interference because they then have better electromagnetic compatibility specifications. A servo cable is therefore much more complex than a motor cable and also has many more cores. The additionally shielded control pairs mean that the cable is no longer as symmetrical as a motor cable, for example. This poses a particular challenge for the design of a high-quality cable. The solution is the gusset-filling extruded inner jacket, which provides a firm foundation for the shielding and wraps around the additionally shielded control pair, guiding the cores lengthwise. The inner jacket is especially important here, since it is the only way to achieve long core service life and guarantee durability for the high-quality shielding. Long travel distances and small bend radii put even more strain on the cable, so that special protection must be provided. 
Find more information about chainflex® servo cables

Reduce installation space by up to 32% – measuring system cables

Measuring system cables are often referred to as feedback or encoder cables. They are used for signal feedback from the transmitter system to the frequency converter. Information such as speed and angular position is transmitted at high density through various signal core combinations in the cable. This means a colourful mix of various cross section, core number and shielding combinations that require special protection during movement. This is achieved with special pair shields or element jackets.
Long travels and small bend radii pose a special challenge, since that is where extreme forces act on the cable. The sensitive components in the cable make it important to use especially high-quality, selected materials in measuring system cable manufacture. High-quality materials such as TPE, a continuously gusset-filling extruded, robust inner jacket, a particularly closely woven shield with high coverage and an optimal braid angle are essential components of a durable, fail-safe measuring system cable. 

Find more information about chainflex® measuring system cables
Measuring system cables for drive technology

chainflex® cable white paper

MicrosoftTeams-image (131).png

You can download the white paper free of charge by clicking on the link below. In the white paper you will find lots of interesting facts about our chainflex® cables and how smaller can actually be better. 
You can learn about the extensive testing process and find out which approvals the cables have. 

 

Consulting

I would be happy to answer your questions

Shipping and consultation

In person:

Monday to Friday from 8am - 8pm.

Online:

24h


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "RCYL", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus SE & Co. KG or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® SE & Co. KG