The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
轻松配置:适用于极端工况的igus不锈钢丝杠模组25/08/2017
drylin SHT 是运动塑料专家igus 十多年来一直为客户提供的保持精确、安静和平稳运行的产品,它的使用寿命非常长。为了进一步拓展这个产品系列,igus现在提供由不锈钢制成的型号。从丝杠模组的轴和滑块,到轴端支承,所有组件均由304不锈钢制成。移动部件采用的则是经摩擦优化的工程塑料。对于工程塑料的原材料,用户拥有很多选择,例如iglidur X 可以让丝杠模组适应200°C的高温工况且具有耐化学性,而食品级材料iglidur A180 非常适合食品和包装技术行业。和所有igus产品一样,新的丝杠模组也完全无需外部润滑。而且新的不锈钢丝杠模组的结构和其他drylin丝杠模组一样,可以由客户自由选择行程长度,以及手轮或电机驱动,从而找到适合自己应用的并可迅速安装的解决方案。根据用户需求,传动销也可以和销、槽或键表面一起提供。 使用drylin SHT 在线配置器轻松满足各种要求 新的丝杠模组拥有四种不同的安装尺寸,轴直径分别为8、12、20和30毫米。对于螺纹,用户可以选择自锁梯形螺纹或高速大螺距螺纹。螺距在2至100毫米之间的丝杠,还有右旋、左旋或正反牙螺纹可选。igus的drylin直线驱动技术部主管Stefan Niermann表示:“为了能够概览所有选项并为每一种工况配置最优组合,我们现在为客户提供了全新的drylin SHT 配置器。这款方便的在线工具简化了丝杠模组的选择、配置和订购流程,只需点击几下鼠标即可。”选择所需产品后,用户会看到所选产品的文档及其配置的丝杠模组的3D视图(也可下载STEP格式),同时可以直接看到产品价格和交付时间,确认后即可加入购物篮。igus目前还在研发一种由极耐腐蚀和耐酸的V4A材料制成的drylin SHT-ES,以适应更为极端的工况。 |