The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
用igus e-rib安全加固 波纹管系统15/11/2017
无论是在汽车行业、机械工程、设备制造还是拣选放置应用中,波纹软管和波纹管系统都被普遍用于保护和引导供应能量、数据、液体和气体的电缆和软管。自支撑波纹管系统具有良好的经济效益,可以确保在机械要求不超过特定限制的应用中有效供能。然而,波纹管系统在高速动态应用中, 一旦超过限定长度就可能导致横向偏转,从而造成波纹管损坏和故障; 对于垂直应用中的波纹管,在最坏情况下则可能因此破裂,从而导致机器或设备故障。针对上述应用,现有的波纹管需要进行加强。而igus的加强件e-rib就是一个安全简单的解决方案。 e-rib助力波纹管实现高速运动 e-rib可以轻松地夹在传统波纹软管上并固定,并且可以从上侧或者外侧连接波纹管的接头。这样可以使波纹管固定地沿一个方向运动。又因为e-rib的两端安装有紧固支架,可以加强软管安全性的同时引导高动态运动下的电缆。即使在多个波纹管并排排布的情况下,e-rib也能够实现可靠的引导。e-rib的稳定性也更高,可以防止内部的电缆和软管过度弯曲,消除电缆的扭结,避免机器故障。所以,易于安装的e-rib仅需几步就能升级现有应用,完成改装。e-rib目前有四种尺寸现货供应,适用于标称直径NW23、NW29、NW36和NW48的软管。 通过视频,您可以对e-rib的功能原理有所了解:www.igus.com.cn/e-rib。 |