The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
首届低成本机器人创意大赛:省时的机器人解决方案赢得评委青睐08/12/2017
在首届低成本机器人大赛上,十二个参赛作品展现了各种各样的创新想法,从3D打印的自动化生产单元到移动抓取机器人,令人大开眼界。它们的共同点就是使用低成本的机器人来实现简单任务的自动化,从而节省时间和金钱。令人印象最深的参赛作品来自冠军得主MLC-Engineering公司,他们将igus robolink关节臂与光学测量技术相融合。这个高性价比的5轴机器人售价3579欧元,可从生产设备上抓取加工完成的元件并传送到光学测量设备上, 并在光学测量设备上对工件进行多次位置调整,以此检测所有相关尺寸。然后,机器人将检测数值输入控制系统,控制系统据此作出“优/劣”评估。最后,robolink机器人根据评估结果来将工件放到传送带上或扔进废件箱。简单任务的自动化具有显著的成效:可以让员工全身心的投入到更复杂的任务中,并可缩短周期, 最终可节省76%的时间。 Motek 展览会上的颁奖仪式 MLC-Engineering公司的创意征服了由研发、专业媒体和制造领域人士组成的评委会。他们大胆创新、精益求精和追求极致的精神赢得了大家的一致好评。igus在Motek展会上举行了首届低成本机器人创意大赛的颁奖仪式,并为荣获一等奖的Michael Lamber颁奖,奖品为一个robolink关节臂的代金券或价值3000欧元的同类机器人组件。二等奖则由霍布商业和家庭经济学院获得,奖品价值500欧元。在学院机械工程系的“国家认证技术人员”课程上,学生们提出了改造曲柄压力机的想法,从而实现自动输送芯片、按指定大小打孔并取出工件成品的任务。简单来说就是吸取打好孔的芯片,然后按照指定位置放置, 即芯片的吸取、定位和放置未来都将由机器人实现。 |