The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
igus推出兼具滑动和滚动运行的模块化E4.1拖链13/04/2018
通常,在10到50米之间的行程应用中,我们会选择用滑行拖链。然而,客户对拖链系统的动态性能和承受移动负载能力的要求不断提升,是目前现有的拖链系统面临的挑战。例如,如果机器的循环速率增加,则拖链的移动速度就要加快,结果就是导致滑行系统达到极限。因此,运动塑料专家igus新增了滚轮链节,对E4.1拖链的标准模块化系列进行扩充。igus副总裁兼拖链部门主管Michael Blaß表示:“新开发的滚轮链节是独立的,滚轮位于链节的中间。这意味着所有链节的节距相同,能够确保拖链系统更安静的运行。”这主要是通过新型的空心滚轮实现的。它们采用了新的几何模型和材料,因此在运动中会减少振动和噪音的产生。在过去多年的测试中,igus的工程师发现了可在6米/秒的速度下安全可靠运行的理想的拖链解决方案。 为了进一步减少运行噪音,滚轮链节在滚轮的前后都有个小斜面,这样在拖链运行时可以避免较大的冲击。滚轮不是易丢失的附加部件,而是以节省空间的方式牢固地集成到链节中。 应用范围极广的“全能模块化系统” 通用的模块化E4.1拖链中的滚轮链节可以让客户轻松地将其机器的拖链系统从滑动运行切换到滚动运行,从而减少驱动力。而且,无需更换新的导槽系统、内部分隔和接头。得益于该系列的模块化特性,还提供有多种不同尺寸和类型。也无需适配链节。滚轮链节可安装在链条的左侧和右侧,易于集成装配。 此外,E4.1系列的所有链节的内部轮廓都非常光滑,其横杆和盖板都是弧形设计,在运行时可减少对电缆的磨损。同时,E4.1拖链系列非常坚固,是专为严苛工况和高负载应用设计的。因此,它们适用于机床、港口起重机等许多不同的应用和行业。配合具有预测性的可靠的isense系列产品使用,还可以避免机器的意外停机。 |