Press

Do you have any questions? Need material?
Current press information and ready to publish photo material is available for download here.
We would also be delighted about your call, e-mail or fax!
 
Press contactWould you like to be added to our media distribution list?

Press releases by area

igus 耐磨带条让滑动更轻松顺畅09/01/2019

任何需要光滑、安静、简单和免润滑滑动的应用,都可以使用 igus 的薄膜款耐磨带条。所以,igus 耐磨带条已被用于家具制造应用,例如调节结构。在大量尘土和碎屑纷飞的木材行业中,iglidur 耐磨带条也展示了其优异性能。例如在锯子切割木板边缘时,使用耐磨带条可以确保旋转挡块在锯片上轻松移动。而且 iglidur 耐磨带条100%免润滑,所以锯末不会粘在导向装置上。为了进一步延长耐磨带条的使用寿命,运动塑料专家 igus 还研发了背胶。现在,这款新型粘合剂更好地提升了耐磨带条的附着力。而且这款新型粘合剂符合 FDA 标准,适用于食品工业。 比标准材料更高的耐磨性 iglidur 耐磨带条在占地超过 2,750 平方米的 igus 内部测试实验室中验证了其极高的耐磨性。在保护不锈钢销的磨损测试中,四款由 iglidur 工程塑料制成的耐磨带条的评分值都要比 PTFE 玻璃纤维和 PTFE 青铜化合物制成的耐磨带条高出 10 倍。除此之外,iglidur 耐磨带条还拥有低磨损、免润滑和免维护的优点。 适用于不同应用的四种高性能工程塑料 由符合 FDA 标准的 iglidur A160 材料制成的耐磨带条对介质具有超高抗性,且符合食品行业对卫生和安全的严格要求。这款材料采用了易于辨识的蓝色。B160 材料拥有超高耐磨性。黑色的 iglidur B160 耐磨带条可以完美融入到可见区域,例如家具上。W160 材料则是专为卫生要求极高的行业应用而开发的,可用于牙科光固化机和消毒机。 此外,iglidur W160 材料含有在紫外线下稳定的添加剂,这一特性使其即使在光诱导氧化中也不会改变性能。第四种耐磨带条是由耐高温专家 iglidur V400 材料制成的。这款材料具有超高的耐热性,可以在高达 200 ℃ 的温度下使用,在 160 ℃ 下仍有粘合力。因此由它制成的耐磨带条的耐磨性极高,适合用于高负荷和高温应用,且耐各种介质。 为不同应用提供不同尺寸 iglidur 耐磨带条适用性广泛,且易于切割。其中,A160、B160 和 W160 三种型号的标准宽度为 20、50、100 和 500 毫米四种,厚度为 0.5 和 1 毫米两种。V400 型号的标准宽度则为 120 毫米,厚度为 0.5 毫米。所有耐磨带条都有背胶可选。此外,igus 还提供特殊形状和宽度的耐磨带条。   新闻联系: 王波 市场部经理 易格斯拖链轴承仓储贸易(上海)有限公司 中国(上海)自由贸易试验区德堡路11号46号厂房A部位 200131 上海 电话:+86 - 21 - 5130 3134 传真:+86 - 21 - 5130 3233 andywang@igus.com.cn www.igus.com.cn/press 关于易格斯: igus GmbH是国际领先的拖链系统和工程塑料滑动轴承制造商。该家族公司总部位于科隆,业务遍布35个国家和地区,全球员工约3,800人。2017年,igus面向运动应用的运动塑料达到6.90亿欧元的销售额。igus运营着业内最大的测试实验室和工程,根据客户需求提供创新产品和解决方案,并快速交付。 "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain-systems", "e-ketten", "e-kettensysteme", "e-skin", "flizz", "ibow", "igear", "iglide", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xiros"是igus® GmbH/科隆在德意志联邦共和国以及国际一些国家中受法律保护的商标。


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH