The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
igus通过自制高温3D打印机推进耐高温线材的开发15/07/2019
高温不仅给工厂中的许多机器元件带来了难题,也给常规的3D打印机带来了挑战。为了将新开发出来的耐高温线材打印成适用于高温应用的耐磨部件,igus制造了一台高温3D打印机。在这款打印机的机械系统中,igus工程师采用了由耐高温不锈钢制成的免维护drylin W直线导向装置,在X、Y和Z轴上则采用了可平滑运行的dryspin大螺距螺纹丝杠。其中,由耐磨的高性能塑料iglidur X和iglidur C500制成的免润滑垫片和丝杠螺母,确保了打印平台即使在内部温度高达200℃时依然可以精确定位。“在新的3D打印机中,我们采用igus的标准组件进行搭建。即使在高温工况下,这些组件依然可以可靠工作。我们使用的喷嘴可以在高达400℃的温度下熔化线材。”德国igus公司增材制造部主管Tom Krause解释道,“为此,我们还开发出了适用于高温工况的新线材iglidur J350,并对它进行了广泛的测试。” 适用于180℃高温工况的耐磨部件 运动塑料专家igus在其滑动轴承和原料棒系列中新增了免润滑的iglidur J350材料。该高性能塑料最主要的特点是极高的耐磨性和对钢的低摩擦系数。它特别适合用于旋转运动,并且在180℃的高温下也具有高度的尺寸稳定性。此外,iglidur J350可以轻松承受中高等级的载荷。这款高温3D打印机还配备了PET膜印板,可以实现线材的高效处理。新线材的典型应用领域包括自动售货机技术、汽车、玻璃工业和机械工程等。除了iglidur J350外,igus还提供另外六种线材,性能从可与食品直接接触的卫生级到抗化学性的化学级不一而足。新iglidur J350丝线可在在线商店订购。 图片说明: 图片 PM7018-1 自制的高温3D打印机采用了带不锈钢导轨的drylin直线导向装置和dryspin丝杠,并可搭配igus新开发的耐高温耐磨线材J350进行打印。(来源:igus GmbH) 新闻联系: 王波 市场部经理 易格斯拖链轴承仓储贸易(上海)有限公司 中国(上海)自由贸易试验区德堡路11号46号厂房A部位 200131 上海 电话:+86 - 21 - 5130 3134 传真:+86 - 21 - 5130 3233 andywang@igus.com.cn www.igus.com.cn/press 关于易格斯: igus GmbH是国际领先的拖链系统和工程塑料滑动轴承制造商。该家族公司总部位于科隆,业务遍布35个国家和地区,全球员工约4,150人。2018年,igus面向运动应用的运动塑料达到7.48亿欧元的销售额。igus运营着业内最大的测试实验室和工程,根据客户需求提供创新产品和解决方案,并快速交付。 |