Triple iF Design Awards for igus products15/03/2016

Since 1987, igus has been awarded a total of 35 iF Design Awards for its wide range of motion plastic solutions. The three most recent awards for innovative product design have been collected for the Triflex RSE robotic retraction system, CFRIP cable stripping system, and the e-bone headphone cable management tool. The iF Design Awards are regarded among the largest and most important design awards worldwide, with a history reaching back to the 1950’s, awarded by a jury of industry and design experts from across the globe.

Secure and flexible Triflex RSE retraction system

The Triflex RSE system enable guidance of cables and hoses on industrial robots to carry cables, as well as solid items, such as rivets or screws, both securely, and cost-effectively. The RSE system guarantees minimum bending radii of the multi-axis Triflex Energy Chain, avoiding the formation of loops or tangling. Elastic cords automatically retract the cable carrier on the transport carriage, while the lightweight, simple-filling plastic carrier follows the robotic movement.

Easy cable stripping with CFRIP

Quick and easy installation of cables is enabled by igus’ CFRIP system. Chainflex cables can be stripped quickly and cleanly thanks to a rip cord integrated into the cable jacket. The unique stripping system for Chainflex continuous-flex cables is suitable for long cable lengths, completely avoiding damage to the cable core structure, even under high dynamics. Using the integrated cord, the cable jacket can be opened precisely to the desired length and removed without any additional tools, saving up to 50% of work time when fitting cables.

New from igus – the flexible e-bone prevents cable clutter outside the industrial atmosphere

Despite its departure from traditional developments from igus, the e-bone headphone caddy proved worthy to the iF Design Award jury. Eliminating the regular occurrence of knotted headphone cables, the e-bone provides an elegant solution that is both flexible and robust enough to stand up to daily use. Earpieces of the headphones are secured into special eyelets, while the cables are wrapped around the compact e-bone body, leaving a secure package small enough to fit into any pocket. While in use, the e-bone can remain on the headphone cables, making re-wrapping quick and easy.

To see all igus iF award winning products, please visit www.ifworlddesignguide.com/profile/736-igus or www.igus.com


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH