My contact person
igus® Ltd.

Caswell Road

Northampton, NN4 7PW

01604 677240

Search for application examples

Improve technology and reduce costs

For years the igus® motto has been "plastics for longer life®". By this we mean the production of innovative plastic products which reduce maintenance work, achieve technical improvements, at the same time as reducing costs and increasing service life, everything delivered immediately from stock.

Our customers were able to improve the technology and reduce costs in more than 590 applications.
Some examples:

Longest travel in the world - no more downtimes

The longest travel with plastic energy chain  

The e-chain systems® today clearly contribute toward reliability, as system downtimes, for example through cable breaks, are reduced to zero.

Cables defy heat, sun, rain and snow

LED screen  

Previously used cables from a competitor had failed; since then the temperature-resistant chainflex® cables are used; the larger-than-life size LED screen in Dallas functions in any weather.

Rough environment, high speed

Special machine construction  

Even in particularly aggressive ambient conditions like in this high speed machining center, energy supply systems prove their reliability.

Costs saved, machine
availability increased

Beverages industry  

As iglidur® plain bearings have a long service life, and in addition need not be lubricated and costs only a fraction compared to conventional bearings, 90% of the costs could be saved.

More than Euro 10,000 saved each year

Fully automatic tire fitting lines  

The previously used bearings were blocked and the shafts used to break. The lubricant-free igubal® flange bearings used instead have been operating since May 2007 without failure. This saved Euro 2,440 in repair costs and Euro 8,400 in machine stoppages each year.

Trouble-free operation instead of shaft destruction

Concrete pipe cutter  

Due to the dirt accumulation in the ball bearings, the balls were blocked and the shafts were destroyed. The concrete cutting machine has now run for over three years entirely free of troubles despite the extremely heavy-duty operation.

Search

Are you looking for practically tested application examples in a certain industry?
Here you can browse through already implemented applications and filter them according to your specifications.

Industry sector:
Case of application:


Heavy fillings

e-chains® for heavy-duty uses: Guiding of the supply cables of a quenching chamber, which moves toward the linked vacuum ovens.

Heavy fillings    

Adhesive resin system

In the case of this adhesive resin system, a lifting platform moves upwardto a height three or four times a day to empty barrels with a volume ofapprox. 200 litres.

Adhesive resin system    

Plastic e-chains® replace steel versions

After six months they used to be finished; finally no more failure thanks to plastic e-chains®.

Plastic e-chains® replace steel versions    

Screen lifter for large displays

Lifting heavy loads

Screen lifter for large displays    

Hand-operated water pump

Resistant to wind and rain

Hand-operated water pump    

Ship-to-shore-crane

This ship-to-shore crane can not only lift the container and set it down again, the whole crane girder can be moved vertically

Ship-to-shore-crane    

Control robot

This robot in a car factory is the “supervisor” over five smaller robots that supply it.

Control robot    

Sludge treatment

The largest plastic e-chain® in the world, the E4.350, is used for this application.

Sludge treatment    

Movable melting furnace

The special requirement with this furnace system was the movement of the filled furnace weighing a total of 45 tonnes.

Movable melting furnace    

Shrinking machine

The challenge was to find a linear guide that can work reliably and quickly under these tough conditions.

Shrinking machine    

Assembly robot

The stones used can weigh anything up to 4,000 kilogrammes. This means a heavy-duty load for all the components used.

Assembly robot    

Jetpack

Since temperatures of several hundred degrees Celsius occur here, the pilot must wear fire and heat-resistant clothing. The bearings used also have to withstand the high temperatures and pressures.

Jetpack    

Testing equipment for trains

Trains are tested for their electro-magnetic compatibility in a shielded hall here.

Testing equipment for trains    

Collision Avoidance
System]

These applications test systems that will make driving cars safer.

Collision Avoidance  System]    

Transporter for steel coils

Heavy steel coils are transported here. The energy supply is recessed into the floor.

Transporter for steel coils    

Anti-magnetic linear drive

An innovative linear drive for transporting loads with or without guides.

Anti-magnetic linear drive    

Assembly robot

This robot lifts heavy work pieces weighing up to 1.7 tons.

Assembly robot    

Mounted sweepers

Maintenance-free polymer plain bearings for rugged mounted sweepers

Mounted sweepers    

Bottling plants

Positioning with maintenance-free igus® lead screw units.

Bottling plants    

Stage hoist

drylin® W linear guides in a lifting platform for concert hall.

Stage hoist    

Container cranes at the CTA

Energy and signal supply to the container cranes at the HHLA Container Terminal Altenwerder - twelve trouble-free years

Container cranes at the CTA    

BANG Kransysteme

Heat and dust: energy supply in adverse conditions

BANG Kransysteme    

Robotics

These modules are parallelogram connections that are designed as modular robot drives.

Robotics    

Lifting platforms

readychain® harnessed energy chains from igus enable safe and precise working at a great height as well as faster maintenance.

Lifting platforms    

Shore power connections

At the Mongstad offshore base, flexible harnessed energy supply systems enable 3,000 shore-power connections per year.

Shore power connections    

Automation solution

Harnessed energy supply systems ensure reliable automatic loading of machining centres.

Automation solution    

Farm loaders

The iglidur plain bearings are used in farm loaders at various locations. Thanks to their specifications, you save costs and time right from the production stage.

Farm loaders    

readycable® in intralogistics

Energy chains from igus® with industrial plug-in connectors from HARTING supply storage and retrieval units from the intralogistics specialist SSI Schäfer

readycable® in intralogistics    

readycable® in special machine construction

Pre-assembled energy supply systems with igus readycable® achieve desired savings potentials in process costs

readycable® in special machine construction    
Applications overview

I have the following project - following question - following request

No application example has been found here for your special case of application. Would you like to have further assistance?
Please let us know how we can help you!



Contact details

Please always complete the fields marked *.

Company:*
First name:*
Last name:*
Phone:
Email:*
We need your post code and country so that we can forward your requests to the right contact person
Postcode:*
Country:*
To receive your free sample or catalogue please enter your address here:
Form of address:
Street:
Town:
State:
Yes, I would like to receive information on current products and services of igus® by e-mail. I agree to the exclusive use of my data by igus® in the framework of advertising messages in accordance with the data protection regulations. I am aware that I can withdraw my consent prospectively at any time by means of the "Unsubscribe" link contained in every e-mail.
I agree to the data protection regulations and the processing of my data. You can revoke this authorisation at any time.
Send