chainflex® cables for use in the offshore industry

Unique throughout the world: chainflex® cables with "DNV-GL" approval

New test stand for cables in moving applications guarantees reliability in maritime use

To enable cables to be used for moving applications on ships and in offshore applications without the need for time-consuming and cost-intensive special approvals, igus® GmbH and the DNV-GL classification company jointly developed a new test stand with the result that a total of 403 chainflex® cables from igus® have now received type approval for permanent movement in e-chains®. These are therefore the world's first cables that are specifically for use in energy chains and have received this certificate.

chainflex® cables with DNV-GL approval  

In order to supply safe and suitable products for these applications, igus® GmbH from Cologne worked with the DNV-GL classification company to develop a new testing procedure and to have their chainflex® cables certified.
 
Development of new test procedures necessaryClassification companies such as DNV-GL typically issue approvals that are in line with international standards. In many cases, especially in terms of the materials, these standards refer to many properties in respect of fire behaviour or other requirements.
Over a long certification time of more than three years with very different areas of investigation, the special knowledge of the two companies led to a situation where cables were designated for use in energy chains on ships and in offshore applications for the very first time.

MUD-beständig according to NEK606

NEK 606 is a Norwegian standard for all cables used in offshore applications. 301 chainflex® cables from igus® are complied with the requirements of the NEK 606 standard.

NEK 606 mud resistant  

Control cables

CF77.UL.D - control cable

CF77.UL.D - control cable  

CF78.UL - control cable

CF78.UL - control cable  

CF2 - control cable

CF2 - control cable  

CF9.UL - control cable

CF9.UL  

CF10.UL - control cable

CF10.UL  

Data cables

CF112 - data cable

CF112 - data cable  

CF211.PUR - data cable

CF211.PUR  

CF240.PUR - data cable

CF240.PUR  

Bus cables

CFBUS.PUR - Bus cable

CFBUS.PUR  

CFBUS - bus cable

CFBUS  

Fibre-optic cable (FOC) PUR

CFLG.LB. PUR - fibre optic cable

CFLG.LB. PUR  

Measuring system cables

CF113.D - measuring system cable

CF113.D - measuring system cable  

CF111.D - measuring system cable

CF111.D  

Servo cables

CF270.UL.D servo cable

CF270 - servo cable  

CF27. D - servo cable

CF27. D - servo cable  

Motor cables

CF27.D - motor cable

CF27.D  

CF34.UL.D - motor cable

CF34.UL.D  

CF35.UL - motor cable

CF35.UL  

CF270.UL.D - motor cable

CF270.UL.D  

CFPE - motor cable

CFPE  

CF310.UL - motor cable

CF310.UL  

CF300.UL.D - motor cable

CF300.UL.D  

More interesting information

chainflex® test lab

Some 700 tests are being run in parallel at the test laboratory covering 2,750 m2, the largest of its kind for testing flexible cables.

chainflex® test lab    

chainflex cables - product overview

Inform, select and order online.

chainflex cables - product overview    

igus® contact Tel: +44(0)1604 677240
Fax:+44(0)1604 677242
Send e-mail to igus®

myigus myCatalog
No minimum order value
800 - 800 Delivery+Consultation Delivery from 24h* Free samples

More than 100,000 products available! Delivery and Customer Service Mon-Fri from 8am-8pm and Sat from 8am-12pm!

Newsletter Registration
Terms and Conditions Imprint General Information Data Privacy Protection Declaration